Other Parts Discussed in Thread: THS3215
Tool/software:
I have two, differential, baseband signals, coming from the output of two different down-conversion mixers. They are 1Vpp, 30 Ohm source impedance, and they go through a set of lumped-element filters. They then become:
- First Signal: 10-60 MHz (useful frequency content would be 30 MHz +- 1 MHz)
- Second Signal: 60-110 MHz (useful frequency content would be 80 MHz +- 1 MHz)
As my ADC does 250 MSPS, I would like to sample them both using a single ADC (and then process them in the DSP). To do that, I think I need to:
- Buffer the output of the differential signals (2x TI buffers)
- Use a non-inverting, summing op-amp to merge the two signals together, as they have different frequency contents (1x TI differential amplifier)
- Probably use the same component as (2) to drive the ADC.
As I can vary the amplitude of the baseband signals, I don't think I need variable gain at the second stage (non-inverting sum). I think this is what I need to achieve:

This is not the smartest question, but can this be done with any differential amplifier/adc driver TI offers?
What about the buffer, any suggestion for the part number?
Thank you!