Part Number: OPA818
Tool/software:
Hi I have a design using the OPA818 where I need to use a sliding rail to add a DC offset to the part. All works fine until V+>11V, Vgnd=+6V and V-=+1V at which point negative rail current begins to increase presumably from the substrate via the thermal pad ESD protection diodes to board ground. So my questions are is the device substrate tied to the -Ve supply rail ? (doesn't say on the datasheet). Also what solution do you recommend? Currently was thinking of tying EP to the virtual ground so that it too slides with the supply pins unless you have a better idea ? Thanks, Steve