Part Number: TLV1841
Tool/software:
Hi all!
I did a simulation using the Spice model of TLV1841 in an application where "reaction time", i.e. propagation delay is critical.
- The datasheet specifies a tpd of about 65ns for a supply voltage of 12V and an input overdrive of 100mV.
- A comment in the spice model says: "Propagation Delay (typical 75ns)"
In my simulation I did a ramp on the input and measured the propagation delay for a 100mV overdrive (see picture attached). I get a tpd of more than 350ns which is way more than suggested by the datasheet and the spice model notes.
Any ideas?
P.S.: in the screenshot you see the green line which is the difference voltage on the comparator inputs, i.e. (Vin+ - Vin-), the left cursor is at a difference voltaeg of 100mV (100mV overdrive) , the right cursor is at the point where the output (red line) starts to react. Seems like I get ~320ns propagation delay)