Part Number: TPA3255EVM
Other Parts Discussed in Thread: TPA3255
Tool/software:
Hi,
This is a two part question:
1--Since the TPA3255EVM has an input buffer built in, I assume using a simple passive preamp with a stepped attenuator on the EVM is fine. If so, is there an ideal value or range for the resistance of the attenuator? I currently have a 48 step series stereo stepped attenuator that is 10k ohms, but I have a 48 step stereo shunt attenuator available that is 100k ohms-- any advantage or disadvantage to using one or the other?
2--Also, this design may only involve having only a single stereo input with this same passive setup. This signal will be coming from a device with a balanced stereo output. Since there be no input selector circuit in the signal path, can I send the balanced stereo signal directly to the EVM's differential inputs via a stereo attenuator? So the volume attenuator would be wired directly between the balanced source and the EVM module.
Thanks
Jack