Part Number: OPA690
Other Parts Discussed in Thread: OPA357, , LMH13000
Tool/software:
Hello team. I have built a driver for a laser diode on OPA690. The control signal is a sine wave 40 kHz, 1.8 V. The thing is that at the output there is only a sine signal, but the laser does not light up. But without the transistor, everything works fine. At the output of the second microcircuit, I get a clean sine wave signal without distortion and 190 mA. What error do you see? The thing is that when I change the microcircuit to OPA357 and transfer the second cascade to a single-polar power supply, everything works fine. But I need the whole circuit to work from a bipolar power supply. Please help me figure this out.