This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6554: Request for Guidance on LMH6554LEE/NOPB Differential Amplifier Configuration

Part Number: LMH6554
Other Parts Discussed in Thread: INA333

Tool/software:

Dear Sir,

We are using the LMH6554LEE/NOPB differential amplifier in our custom project.
In our design, we feed a 3.8 GHz RF signal into an RF power detector (LT5538).
The power detector provides an output voltage corresponding to the input RF power level.
This output is then passed through a differential amplifier and a filter, and finally fed into the ADC inside the STM32 microcontroller.

Could you please suggest whether we should use AC coupling or DC coupling between the LT5538 and the LMH6554LEE/NOPB?
Also, could you recommend a suitable reference circuit for configuring the LMH6554LEE/NOPB?
The amplifier should only amplify the output signal of the power detector and should not amplify or shift the ADC reference voltage (offset).

Thank you for your support.

Best regards,

Samudralankaiah.

.