This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA500: TINA_TI simulated TI Op Amp and TI Diff Amp's Vsat_low goes below lower supply rail

Part Number: INA500
Other Parts Discussed in Thread: TLV9042, OPA170, INA132, , TLV9041, TINA-TI

Tool/software:

Dear TI,
I believe there is a behavioral model simulation quirk where TI op amp output at Vsat_low goes below the lower bias rail even without an external negative stimulus.

I created the simple TI_TINA comparison circuit, below, to understand the lower-rail saturation mV of several TI diff amp configurations. 

Both input stimulus are positive, and both well within the supply rails.
Pos = 900mV; Neg = 1000mV, e.g., a -100mV difference.  VEE = GND, VCC = 5V.

The two op-amps have external resistors added to give them similar diff-amp behavior as the INA parts. 

At light/no load, I would expect an output of ~0.00V to several or tens of mV positive of the negative rail, which is what I bench-measure on real parts.
Strangely, the INA500A, INA132, TLV9042 and OPA170 outputs all go slightly negative (two go to -3mV. Two go to -7mV).
This is unexpected, as there is no actual source of negative voltage on the surrounding circuit, and the negative bias rail is at ground.


Please advise and/or update the model as needed.

--Peter Wahl

  • Hey Peter,

    Thank you for finding this error! I will report this to the engineers responsible for each of those SPICE models (different devices are supported by different teams) so they may update them appropriately!

    Best,
    Gerasimos

  • Hi Gerasimos - Do we know when a corrected model would be available?

  • Hey Jacob,

    I'm not sure on the timeline here. I will sync with the other teams and let you know if they have a timeline for this. In the meantime I have this entered into our tracking system to make sure this gets corrected.

    Best,
    Gerasimos

  • Hi Peter & Jacob, 

    What was the broader problem being solved via the simulation?
    In the meantime, where you able to arrive at a solution or do you need us to help with evaluation of the INA500 & INA132 in a different way? 

    All the best,
    Carolina

  • Caroline,
    The INA500A is used in many places in my design. In most circuit use cases, the signal output is kept ~100mV above the lower rail, so no big deal.
    However, in the particular use case it does matter. I am simulating a INA500A pair used as an offset-corrector and full-wave-rectifier for a hall sensor (0A gives 2.5Vout).

    In this FWR app, a pair of INA500A's are summed, where one is sending a half-wave and one is at Sat_low, depending on if the signal is > or < 2.5V. The two outputs are resistively summed for the output signal. This avoids the classic diode approach and its Vfwd limitations on output range and resistor matching hassles. The sat low value has some small effect (a few percent) on my full-scale signal. Generally, I do not need high fidelity down near zero, but it is that sat low is skewing the results due to the summing node action. I have also noticed that the Vsat low can have abrupt ~10mV steps with small load changes. This also seems unlike what I would be expected from an actual part.

    My present work around is simply to test one direction at a time and use a simple 7mV source to replicate the other INA500A that nominally expected Vsat at that time.
    (not -7mV, i.e., below Vee.) 

    My work around will do fine for the next few weeks, but I do have a top-tier customer-facing CDR in about a month.
    I would rather not have to explain my patch to the customer.

    --Peter

  • Hey Peter,

    I poked around a little in the model and found an issue that, when resolved, seem to fix the clamp limit. I have not fully run the validation suite of tests on this device, so your mileage may vary, and please let me know if you run into any other unexpected behaviors.

    I've also included another fix that hasn't yet been pushed to the web yet to fix some of the gain peaking issues with the models first rev. This new model will be pushed to the web shortly.

    INA500A.lib

    INA500A_fix.TSM

    Best,
    Gerasimos

  • Thank you for addressing these two (three) issues.
    I will check it out ASAP.

    Also, thank you for fixing the "1.080108MEG" typo (issue #3).


    Till then, just a note:
    This latest clamp and peaking fix, attached above, seems based on the Rev A model from Bali Ravi in 2019.
    Shouldn't these both the clamp and gain peaking fixes be applied onto the latest Rev B 2024 version?

    Regarding Rev A vs Rev B. I much prefer Rev A in that the net list follows a logical progression of circuit netlist flow, i.e., parts of a like net connection are grouped sequentially in the code. The Rev B, by contrast, seems to have been ran through some code-formatter that alphabetized the net components, thus jumbling the logical readability.

    Does Rev B have any real improvements, or is Rev B was just a formatting "update"? 
    I would be great if any substantive changes in the Rev B (including the fixes) were made into a style honoring the Rev A's netlist-readable-first component listing.

    --Peter

  • Hey Peter,

    So, that was a copy-paste error on my side. The core amplifier is based upon the TLV9041 amplifier, with some added resistors on die. The original model for the TLV9041 was used for the creation of the INA500 model. Consequently, this is why the swing outside the rail error is common to the INA500 and TLV9042 model. So this is a little bit of a peek behind Oz's curtain, luckily there's no phony wizard, just some innocuous IP reuse.

    Rev B had an improvement to ease convergence in PSpice for TI, and I believe had another convergence aid added in to help convergence in more complex schematics. Even though this was a fix for PSpice for TI, we rolled out the change across all models for the purpose of standardization. There was no negative impact on the TINA-TI model, and we didn't want someone to copy-paste the netlist from TINA-TI into PSpice for TI or any other Cadence simulator and now start to have convergence problems.

    Also correct that the netlist was run through a formatter that does move the components around, but prevents any repeat component names when converting a hierarchical schematic to a single netlist, and automatically appends the header to the netlist. It is a convenience for those generating the model, but does make the netlist a fair bit less legible.

    I did try to make the same netlist fix in PSpice for TI, but it seemed to cause a convergence error. This will require some more debugging and poking around the model, but surely there is an answer somewhere.

    Best,
    Gerasimos

  • Thank you so much for the transparency and very quick resolution to the issue.
    I greatly appreciate TI's service and great products.