This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS6222: Truth Table

Part Number: THS6222
Other Parts Discussed in Thread: TMUX6222

Tool/software:

Team,

There's a confusing about truth table. 

In the diagram here, it looks like it's a NO state (Normally OPEN). It means when SEL1/2 is set "1", the SW is operated and ON. correct?

But in truth table, it is the opposite, isn't?

Regards

Brian

  • The TMUX6222's description of "active low" means that that the switch is closed (channel on) when the SEL input is 0.

    The block diagram shows the state when SEL is 1. The description, the truth table, and the block diagram are all consistent with each other.