This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH7324: TLV1872

Part Number: LMH7324
Other Parts Discussed in Thread: TLV1872, THS4041, , TLV3601, UCC27517

Tool/software:

Hello,

TLV1872 (65ns, 40V, dual) is too slow compared with ISL55142IVZ.

Is it possible to replace this function with a fast comparator with a maximum propagation delay of 15ns and a Rise time/Fall time < 2ns followed by a 17V powered amplifier? Totem pole output.

Unipolar power supply.

Ex: Can the THS4041 AOP be supplied as a single-pole device with a supply voltage of 17 V?

Thank you for your help

  • The LMH7324 has a differential output. The THS4041 has a slew rate of 0.4 V/ns.

    What are the required input voltage range and propagation delay?

    I would combine a fast comparator with push/pull output like the TLV3601 with a a fast digital buffer like UCC27517, for a total propagation delay of about 15.5 ns.