Other Parts Discussed in Thread: OPA991, TINA-TI
Tool/software:
Hello,
I am working on a current source (100/200mA).
To minimise power losses in the shunt, I've chosen to use an INA180 in the feedback loop.
The system does not require a high bandwidth (10Khz or less).
Doing an AC sweep there is a amplitude ''bump'' between 200Hz and 5Mhz (about). I can reduce the amplitude or the shape of the frequency response but I still get this ''bump''.
The problem that is reflected in the overall noise current transmitted to the load (laser diode), this shows in the laser light FFT, as well as the boost converter (but that is taken care of). I could get read of the INA180 and use a bigger shunt, but I do not want to do that for now.
I suspect it is the INA180A2 reduced BW in the feedback loop and the driver ''integrator'' + Mosfet configuration messing-up the response ?
The question is what to do to reduce the bump...
1. Type II controller (RC// with 47nF) ? how to calculate the values ?
2. Finding a similar INA180A2 op-amp with higher BW, or making one with a faster op-amp
3. Fine tuning the integrator capacitor ? how to calculate.
To be fair, there are a lots of App. Notes on that, but none of any practical REAL use, it is all put together with little finesse and probably never used in the real world.
Thank you for your support.