Part Number: ALM2402-Q1
Other Parts Discussed in Thread: ALM2402F-Q1, , ALM2403-Q1
Tool/software:
The ALM2402Q1 op-amp is to be placed in a circuit with dual supply configuration. There are two pins labeled as ground, and not V- like usual amps, which are to be connected to the negative rail. The EPAD is noted, "It is recommended to connect the Exposed Pad to ground for best thermal performance. Must not be connected to any other pin than ground. However, it can be left floating.". What is the required connection of the EPAD, i.e. 1. attach to negative supply the same as the ground pins 2. Attach to ground separate from the ground pins, 3. attach to copper for thermal dissipation but keep no electrical connection.