Part Number: PGA309EVM-USB
Other Parts Discussed in Thread: PGA309
Tool/software:
Hello,
I would like to use the Tio32.dll to control the USB DAQ platform to control the MultiCal hardware. I am using the Multi cal to calibrate PGA309s. The Calibration step is done, but I want to do some other things that involve manipulating the MultiCal Hardware via the USB DAQ platform. I need to know how to power on a unit and take a reading using the MultiCal hardware.
Two main things I need:
1. Control the multiplexer on the MultiCal in order to take readings with the DMM
So far I have Tio32_RunMnemo(....) and the command is "CMD CTRL ###" but I don't know what number to use.
2. Power on the units using MultiCal hardware
If necessary, I need the PGA309 units to be powered on. If this happens automatically then great. If not then I need to know how to get the multical hardware to do this.
Nathan