Part Number: LMH6702
Other Parts Discussed in Thread: THS4304, OPA695, , LMH6703
Tool/software:
What would be a suitable opamp to use to reduce the amplification ratio to 1/10(Av)?
I want change Input(Vp-p: 1.0V) -->Output( Vp-p: 150mV).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rice,
Our unity-gain stable voltage feedback amplifiers are capable of attenuation (gains lower than 1V/V)
Do you have any other design requirements such as:
Thank you,
Sima
1. +5~ -5 Volt
2. BW : 1.5GHz
3. 10mA < driving
4. unipolar input - unipolar output / offset 1.17V Vamp=120mV
Hello Rice,
I apologize for the long delay here.
If you first requirement on supplies is flexible. I would recommend THS4304 which will be capable of 1/10 attenuation + your 2,3,4 requirement.
Otherwise, another option would be to divide down your signal prior, then use a current-feedback amplifier such as the one linked LMH6702, LMH6703 or OPA695 at unity gain.
Thank you,
Sima