This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA241A: Gain variation wrt input signal's duty cycle

Part Number: INA241A


Tool/software:

Hello,

Please find the below schematic of INA241A2.

During testing , 115mV of signal was fed across IN- and IN+ at TP15 and TP17 points.

With 80% input duty cycle , we are observing output voltage reaches 2.120V where input voltage is 0.115mV (Ideally output had to be 0.115*20 which is 2.3V).

But with  20% input duty cycle , we are observing output voltage reaches 1.89V where input voltage is 0.115mV (Ideally output had to be 0.115*20 which is 2.3V)

Could you please explain why Gain is varying wrt input duty cycle and there is a lot of error in Gain.