Tool/software:
Electro-chemical oxygen sensor output connect to LMP7721, the output of LMP7721 is not right. (output is very high)
Connect a current source to LMP7721, the output of LMP7721 is right.
The output of electro-chemical sensor and current source are same(about 1nA to 1000nA).
The strange thing is, if I connect an old sensor(worked after a long time) which output is several nA, the output of LMP7721 is right.
I guess it is something about impedance.