Part Number: INA236
Tool/software:
Hello TI,
I'm reopening this thread, i have new informations that i think will help pinpointing the issue.
RECAP of other thread :
-Current measured when using only current measurement is very close to actual current.
-When adding the voltage measurement there is a large deviation on the measured current. The longer the sampling time, the closer we get to the actual current.
Setup :
We monitor the current of a high side switch 14V - 0-15A
Rsense = 0.5mohms
Rflt = 100R
Cdiff = 1uF
Sampling time 332us (avg: 64)
Resistive load for 1.4A
New information :
-The filter seems to have a large impact, removing the 1uF solves the issue, a 0.1uF helps but is still too much.
-The error is an offset, at 15A or at 1A, it is around the same delta in mV
Any ideas why the capacitor impacts the measurement, i would like to understand the issue to choose the filtering capacitor and resistors that are the best suited for this application.à
Thank you.