Hello,
Sensor AFE : LMP91000
Parameters : Programmable TIA gain, Internal Zero selection (Reference voltage), variable BIAS voltage, FET switch
I am trying to figure out the proper settings for various toxic gas sensors using LMP91000 eval board. I can read/write configuration registers through I2C interface and was able to verify them with the logic analyzer. I would like to verify the effects of these configuration register settings like programmable internal zero, programmable TIA gain, and variable bias on the LMP91000 eval board before placing any actual sensor. The only parameter i was able to verify is the programmable internal zero which shifts the output scale at the Vout pin. Could someone explain me how these parameter settings affect the 3 electrode pins and help me with simulating a small input range and playing/verifying with these programmable registers in the stand-alone mode ?? I also have the two interface boards -- SPIO4 and ADC161S626BEB for interface with the computer through usb and configured using the WEBENCH graphical user interface.
Thanks,
Raj