Part Number: TLV3601
Other Parts Discussed in Thread: TLV3511, INA185
Tool/software:
Hi,
I am trying to design a current zero crossing detector with TLV3601 based on the following circuit:

However, I found that there is a long delay (~150 nS) between actual current zero crossing and TLV3601 output change, much longer that datasheet specifications.
What can I do to minimize this delay?I need the delay to be <40 nS, preferably <10 nS. I have tried using smaller RC values for the LFP before TLV3601, but it did not help
I noticed that the delay specified in comparator datasheets are usually based on an overdrive voltage of 50 or 100mV, while I may want my comparator to respond at <1 mV input voltage difference. Is this the reason why I am getting much longer than datasheet specified delay?
Is there any comparator that can meet my delay and input voltage requirements? Or will it help if I add a preamplifier stage, similar to the following schematic from TLV3511 datasheet? If yes, which amplifier should I choose? The TLV3511 datasheet does not seems to provide any recommendations for the INA.

Thank you