Part Number: OPA2677
Other Parts Discussed in Thread: TINA-TI
Tool/software:
Hi,
I'm trying to use the OPA2677 current feedback op-amp to drive a large capacitive load (around 10 uF). The op-amp is configured as non-inverting and with a gain of 2x using feedback resistors. I'm concerned that with driving such a large capacitive load, the feedback resistors would have almost no current flowing into them untill this large output capacitance is charged and so the feedback gets delayed?
Can I drive a 10uF load with this op-amp with feedback resistors (Rf = 100k, Rg = 100k)?
is there an LTSpice model for this part?
Thanks