Other Parts Discussed in Thread: ADS4249
Tool/software:
Dear Engineer:
Please help us to confirm the following 3 issues:
Issue 1:In the LMH6554 datasheet(SNOSB30P –OCTOBER 2008–REVISED JANUARY 2015),the CMVR is ±1.3V,the Output Voltage Swing is ±1.42v,I want to konw what is the voltage(±1.3V ±1.42V) refered to? refer to GND or (V+ + V-)/2 ?

Issue 2:In the document 《AN-2177 Using the LMH6554 as an ADC Driver》,the VICM is adjusted to 1.25V,the normal VICM range is ±1.3V in the LMH6554 datasheet,this make the device can only tolerate the signals up to 1.3V-1.25V=50mv。The output voltage swing is ±1.42V,the SE output swing remain 170mV。What's the purpose of adjusting the VICM to 1.25V via pull-up resistors?


Issue3:What is the specified voltage range for the output common-mode voltage(the voltage on the Vcm pin)?