Tool/software:
Hi team,
My customer is considering TLV3201-Q1, and from datasheet there is a note mentioned "Input signals that can swing more than 0.5V beyond the supply rails must be current limited to 10mA or less". Customer think this note is confusing, since it may be interpreted as they can let input signal swing more than (VCC)+0.5V, if the current is limited to 10mA.
Is it correct that customer should keep input voltage within (VCC)+0.5V no matter of any input current? Any reason or background to specify this requirement in the datasheet?
Thank you,
Muwei Zheng