This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP7704-SP: Instrumentation Amplifier-Suggest a suitable amplifier for the attached spec

Part Number: LMP7704-SP

Tool/software:

Instrumentation Amplifier

Sl No

Specification

Value/Range

1

Total number of channels 04 or as per the design

04 or as per the design

2

Input impedance

≥ 50 MΩ, ≤ 5 nF

3

Input Connection

Differential input with floating common

4

Differential mode voltage range

±10mV to ±10V

5

Common mode rejection ratio at gain 1000

90dB or better at DC to 50 Hz

6

Gain

1 to 1000

7

Accuracy

+/- 0.02%

8

Bandwidth

DC to 10kHz

9

Channel isolation

Four port – Galvanic 600VDC

10

Linearity

+/- 0.01%