This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1350: AMC1350

Part Number: AMC1350
Other Parts Discussed in Thread: AMC3330

Tool/software:

Hi, 

is it possible to use the AMC1350 in the following configuration to measure the Neutral Point Displacement? 

  • Hi, 

    Yes this is fine except your VDD1 supply must be referred to GND1. I don't see this circuit on your schematic so I cannot confirm. 

    If this is an issue, AMC3330 may be more appropriate so you don't need an additional isolated power supply. 

  • Well, the VDD1 is an insolated power supply referenced to V_NEUTRAL. 
    So the actual configuration would be this one:



    But i am not sure this will work fine. 


  • Hi Federico, 

    I see, thank you for providing a more complete schematic. Do you need to measure this continuously? 

    As of right now, you have a permanent connection from VAC to Neutral to PE through this resistor divider. 

    You may want to consider adding TPSI2140 type isolated switches such that you can measure Neutral to PE periodically and there is not a continuous current flowing from VAC to PE.