This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH13000: questions for this device

Part Number: LMH13000


Tool/software:

Hi all,

My customer is considering this device.

1) When is the RTM for this device? 2026?

2) Is a sample available?

3) Can this device output a constant current of 5A? The datasheet (see below) says it can output a continuous current of 1A.

'' (1) The LMH13000 continues to operate for VSET greater than the mentioned limits; however, lifetime reliability is not guaranteed.''

Best Regards,

Ryusuke