This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM124: LM124J/883B MM54HC00J MM54HC00J/883 DS26L31MJ SN54LS31MJ 2N1593

Part Number: LM124

Tool/software:

Hi , Can you please confirm the below Part Number Life Cycle Status

LM124J/883B
MM54HC00J
MM54HC00J/883
DS26L31MJ
SN54LS31MJ
2N1593
  • Hi Pradheep,

    , Can you please confirm the below Part Number Life Cycle Status

    LM124J/883B is military and space grade op amp. LM124J can be ordered via the link below. We should be enough in stock for the military and space application, since the wafer is very specified and qualified via for different applications and compliances. 

    https://www.ti.com/product/LM124AQML/part-details/LM124J/883?login-check=true

    LM124 has a completely different requirements. This is the standard op amp and it does not meet the military or space application. It is widely available for commercial purpose. You can tell  by the pricing of the op amp. Recently, new FAB has been introduced in the part, so LM124 has a new design for the FAB change and it will last for another 20 years or more. The new LM124 is totally different LM124J regarding to its FAB, Silicon size and other performance parameters (should be similar). 

    In the list above, you listed several ICs. I can only commend on our op amp products. Some of the products seem to be manufactured from other companies. 

    If you have other questions, please let me know. 

    Best.

    Raymond