This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM139A: More graphs/data on switching timing over temperature ranges?

Part Number: LM139A


Tool/software:

My customer notices that there is a slow down in switching as temperature increases and are interested in data that validates their finding. Over temp range -34 to 85 C.

  • Hello Lauren,

    The datasheet contains these graphs in figures 6-25 to 6-30, and they contain -40°C and 85°C. Prop delay does become longer as the temperature increases.This is typical for a bipolar device.

    The difference between -34 and -40 would be very small. We do not have any more specific data other than what is shown in the graphs. As can be seen, overdrive has the biggest influence of the prop delay.