Part Number: TLV4111
Other Parts Discussed in Thread: ALM2402-Q1, ALM2403-Q1
Tool/software:
I have a requirement to drive a load (a high voltage DC-DC converter). The maximum voltage is 12V and the maximum current required is 300 mA. The output of the DC-DC converter is proportional to the input drive voltage.
My plan was to generate the control voltage with a DAC (0 to 3.3V). That is then amplified as needed, but I have not been able to find any buffer amps that would meet the drive capability. I had started by looking at the TLV4111, but later realized that the requirement goes up to 12V!
Any suggestions? (The simpler, the better.)
Thanks