Other Parts Discussed in Thread: THS4131
The data sheet specifies a max differential input of plus and minus 6
volts. I need to know if this applies to the single ended configuration
at gain of one in the figure on page 18, figure 38 of the data sheet.
That is exactly how I'm using it. I am powering
the device with a bi-polar plus and minus 12 volt supply.
The part works great with an AC signal of 10V peak-to-peak down to about
10Hz. As the frequency goes below this the -Vout output begins to
drop. At DC the -Vout output stays stuck at zero volts.
According to the datasheet the part should work with static DC levels.
I want to give the part an input signal of up to plus and minus 10
volts, DC to 100KHz, powering the THS4131 using a + - 15V supply. Is
this a problem in this configuration? Why is the part not functioning
correctly down to DC?!
I contacted tech support last thursday and I still have not received any answers. Any help is appreciated before I'm forced to move on from a TI solution.
Thank you,
David
617-838-5944