Tool/software:
Hi,
I am simulating Howland charge pump with OPA828. I see the edges are getting chipped off in my output. Any idea on why this could happen?
Thanks,
The input rise time is 10uS and 5V at 100Hz.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I am simulating Howland charge pump with OPA828. I see the edges are getting chipped off in my output. Any idea on why this could happen?
Thanks,
The input rise time is 10uS and 5V at 100Hz.
Hi Binit,
I see the edges are getting chipped off in my output. Any idea on why this could happen?
I see the same behavior in the simulation plot. My opinion is that this may be artificial or dynamic behaviors in the tool (may be in Spice models). I altered the R3 or Rsen values, and found that some square wave output looks fine, especially when current close exceed approx. +/-25mA range. But the OPA828's output Isc is only approx. +/-30mA. All lower output current plots have the "chipped off" plot when it is simulated. It also also looks fine when the input voltage is increased.
OPA828 Howland Isource 05142025.TSC
The V-I behavior is definitely linear when I performed DC sweep of the input signal from -5Vdc to 5Vdc, and it looks fine as it should in static states.
If you have other questions, please let me know.
Best,
Raymond