Tool/software:
HI,Staff
INA133 (SBOS115A) page 7 Settling Time test conditions are Vs = ±15V.
It is specified as 4μs (TYP) when 0.1%, CL = 100pF, and 5.5μus (TYP) when 0.01%, CL = 1000pF.
However, in the graph in Figure 5-18, the values at ±15V are not 4μ and 5.5μs.
It can be read as 4.5μs (TYP) when 0.1%, CL = 100pF, and 8.5μs (TYP) when 0.01%, CL = 1000pF.
What is the difference between the Settling Time test conditions and those in Figure 5-18?


regards
cafain