Tool/software:

Hello, regarding the application of AMC3302, we as above FB1 used spec 182 beads (BLM15HD182SH1) as recommended in the datasheet, R2=R4=100R, shunt=0.1mΩ.
We have the following problem in the application process:
In some high-frequency voltage oscillating conditions, the current through the shunt is 0A, but the shunt In some high-frequency voltage oscillation conditions, the current through the shunt is 0A, but the voltage of the shunt has 100-300kHZ high-frequency jitter, and at this time, the V (OUTP-OUTN) is abnormally high (>3V) for about 10us.
We did the following
Measure 1: Keep FB1/FB2, change FB3 to 0R resistor, V (OUTP-OUTN) ≈ 0V, normal.
Measure 2: Keep FB3, change FB1/FB2 to 0R resistor, V (OUTP-OUTN) ≈ 0V, normal.
The test data is as follows

May I ask.
Q1: What is the principle of measure 1 and measure 2?
Q2: Is it possible to remove the magnetic bead or adjust the parameters?
Q3: What are the resistance values of the following 5 resistors?