This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA381: Current sensing IC recommendation

Guru 12775 points

Part Number: INA381

Tool/software:

Hello,

My customer is looking for a current sense IC that can support the following features.

   - Detects current of 8mA to 20mA (5V) and outputs High(open-drain) or Low level

   - They want to distinguish between cases where there is no current or a very small current flowing and cases where there is 8mA to 20mA flowing.

Could you please recommend the most suitable low-cost solution among TI products to implement this function?

Thank you.

JH