Other Parts Discussed in Thread: THS3491, THS3470
Tool/software:
The BUF634A can be used to drive many typical headsets used for home/commercial use.
Aircraft headsets though use 150/300/600 ohms plus Military use 8 ohms.
The BUF634A does not have enough drive capability to drive 8 ohms hard enough to meet requirements. Maybe parallel two?
If you pick an amp IC for 8 ohms it won't meet the drive requirements of higher impedance headsets.
What system design approach should be taken? Two driver circuits that switch over depending on the connected impedance?
Never seen it done...