Part Number: INA260
Other Parts Discussed in Thread: INA240
Tool/software:
Hi,
My motor jitters when using INA260 to measure its Current.
Does your part work in PWM ?
My motor is 24VDC, driven by PWM between 10% and 100%, and its current (in test mode at no load) is just around 300mA. (and this is when is jittering); and at max load is expected to draw about 7 Amps (didn't test this to see if it jitters or not).
How do you use INA260 in TRIGGERED mode?
The question is NOT how to set it in triggered mode, but what actually is the Trigger that commands another reading?
Thanks.