Part Number: OPA2675
Other Parts Discussed in Thread: LMH13000
Tool/software:
Hi, I want to use high-speed LTTL to load LED for communication. Can I use OPA2675 as the driver? Or is there any better solution?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We have recently released LMH13000 which is more suitable to drive LEDs/Laser for communication. It also supports LVDS, TTL and CMOS logics with very fast rise and fall times for pulsed current-output applications.
Hello ,
can you please help me understand the forward voltage drop , current required to drive the LED for 30W. For example i would need these two parameter to calc if 30W LED can be driven.
The LMH13000 can drive 5A current with say ~ 10 to 15V drop on the load ( which is LED in this case ) since it support upto 18V.
Also can you help me give a spec on square waveform frequency you need on the current output waveform.
LMH13000 can drive up to 250MHz square waveform with 50% duty cycle. will this work to achieve your required communication speed.?
find the datasheet here : datasheet https://www.ti.com/lit/ds/symlink/lmh13000.pdf?ts=1748254002831&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FLMH13000