Part Number: TLV9154
Other Parts Discussed in Thread: TL072H, TLV9164, OPA4197
Tool/software:
Hello,
I'm using this op amp as an analog front-end (unity gain) buffer and it works according to spec for frequencies less than a few kHz.
Above 10-15 kHz, the part's output voltage becomes dependent on the output load - the output signal becomes distorted.
Also, if I use an isolation resistor on the noninverting inputs, output ringing occurs that is also load-dependent.
Please see the attached schematic and traces:

The yellow trace below is the input signal and the blue trace is the output signal.
Here, at 20 kHz, the THD is low and the output is not distorted.
At 40 kHz there appears quite a large distortion at the zero-crossings. This is with a 160-ohm resistive load to GNDA.
Without the 160-ohm load, there is no distortion.
There is also some ringing with the 13k-ohm input resistors. This ringing goes away when the outputs are loaded.
No ringing with the 160-ohm load, but the signal is distorted.
The datasheet states that TLV9154 has a GBW of 4.5 MHz and a slew rate of 20 V/us so this is not what I expected.
If I swap the TLV9154 with a TL072H, the problem goes away, but, of course, TL072H is not a RRIO op amp.
Is this an expected behaviour for this part and if so, does an equivalent part exist that can tolerate up to 30 V of input supply voltage?
Thank you in advance!