Tool/software:
Hi TI team, question regarding current sensor, we have using it in following schematic. 
VCC = 1.76V
VSNS_REF = 0.256V
Resistor R3987 10k disconnected
IN- shorted with IN+ between 7 and 8 pins.
In this setup I should get at output pin5 the input of VSNS_REF right?
But I getting 0.222V that is lower of VFER = 0.256V!
I think that it because of VCC is close to minimum 1.7V but not sure!
Can u help me to clarify this issue pls, maybe there is other things that I don't know or don't see?