Part Number: OPA4991
Tool/software:
Hi Sir :
We are using OPA4991 instrument amplifier for small signal amplification, but we are currently facing a problem. The differential input itself introduces a signal of about 6mv, which has a significant impact on our measurement signal (ranging from 0-100mv). What I can think of now is to use differential input and sacrifice the sampling range to bias the input signal to 100-200mv, reducing interference; The second issue is that the output signal range is -5V to 5V, and the input of the ADC pin at the back can only be -2.5V-2.5V, or 0-3.3V. Using a 3.3V voltage regulator will cause the signal output to attenuate significantly from 2.7V onwards. Is there any other compatible method ?
Is there a better design concept that can provide ?