This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM358: ‌LM358: Connection Methods for Electrical Characteristic Testing of Operational Amplifiers‌

Part Number: LM358

Tool/software:

While reading the LM358 datasheet, I don’t fully understand this statement: "Measured under conditions of VCM = VOUT = VS/2, RL = 10kΩ (connected to VS/2)."

Is the LM358 configured as a voltage follower? Could you please provide a schematic diagram of the op-amp test setup referenced here?

Additionally, what is the purpose of these configuration conditions? Are they meant to ensure the op-amp operates in its linear region?

What is the role of connecting RL to VS/2 in this context?