Other Parts Discussed in Thread: OPA197, OPA192
Tool/software:
Hi all,
My customer uses the following TL081CDR before PCN and uses the offset adjustment function.
I was told them that the offset adjustment function became unavailable around PCN was dated in 6/16/2022.
The number of occurrences is 6 out of 6.
While investigating the cause, I found a related thread.
(+) TL081: TL081CDR - Amplifiers forum - Amplifiers - TI E2E support forums
1) Is the offset adjustment function unavailable because of a change in the IC internal (block diagram) due to a change in the die?
2) If 1) is YES, I think that the function of OFFSET N1 and N2 and the pin handling method changed. Please revise the data sheet.
3) They are looking for a pin to pin replacement. Do you have an opamp with the same pin arrangement? Or do you have a lower offset opamp with the same pin arrangement?
We are looking for a replacement as soon as possible.
Thank you for your help.
Best Regards,
Ryusuke