Tool/software:
Hi, Staff
Please confirm the following two points in the INA133U datasheet (SBOS115A).
1. page6 Vo (Output voltage, gain error < 0.1%)
The negative value is listed as (V+)-0.8, but since it is on the negative side, I think it should be (V-)+0.8.
2. page7 IQ (Quiescent current (per amplifier))
Under TEST CONDITIONS it says Io=0V, but since it's a current, I think the unit should be A, in other words Io=0A.
Is my understanding correct?
I'm sorry it's a small thing.....
regards
cafain