Other Parts Discussed in Thread: TINA-TI, , OPA836
Tool/software:
OPA838IDBV used with a 5V single supply. 5V confirmed at pin5 & 6. Vref is disconnected from any other circuitry.
A simple circuit here, but it doesn't work. 2.5V at the potential divider rises to 3.9V when the op-amp is populated. Vref = 3.9V. The white line on the body aligns with pin1 & 6. Found no reference to how to determine correct orientation using the body markings. Can't see why this doesn't work. Input range is restricted (not rail to rail) but an input of 2.5V should be ok. Baffled.