This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR300: Protection XTR300 with two TVS3300 back to back

Part Number: XTR300
Other Parts Discussed in Thread: TVS3300,

Tool/software:

Hi all,

I would like to know how protect the output XTR300 in current and voltage mode. The power V+ should be 24 V DC and V- should be -5 V DC. So, I've read that the two TVS3300 connects in back to back could be a good choose to protect the device. So, i need if is correct and if was necessary to insert a resettable fuse in series output connection user.

Thanks