Tool/software:
In the datasheet there is a ambiguity about the maximum output current drive capability of the THS3491 amplifier.
In "Section 1: Features" it is mentioned that "Linear output current: ±420 mA (typical)" while in "section 8.1 Absolute Maximum Ratings" it is mentioned that "Continuous output current of ±100 mA" with a clauses of "Long-term continuous current for electro-migration limits".
I would like to know can I use THS3491 amplifier to supply my application with 400mA of load current for 3 to 4 hours continuously, then turn it off for 30 mins and again load it for 3 to 4 hours with 400mA load current?
Thanks in advance for your response.
Regards,
Radhakrishna Pani