Part Number: TLV7011
Other Parts Discussed in Thread: TLV7031,
Tool/software:
Hi team,
Do we have any slide or comparion betweenTLV7031SDCK and TLV7011DCKR ?
My customer is asking about this, thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
To compare devices, go to the search page, select the device with the checkboxes to the left of their name, and click "Compare". Here is the result: https://www.ti.com/compare-products/?id=50002&type=GPT&partList=TLV7011,TLV7031&columnList=480,116,83,358max,358min,2954,2955,1498,2192,1typ,2max,78,1192,769max,261011,1811,1130,81max,81min,3316,-4
The TLV7031 is slower and uses less power; the TLV7031S has shutdown.
Hello Oliver,
The TLV7031 is the micropower version of the TLV7011.
| ► Part Number | TLV7011DCKR | TLV7031DCKR |
| Pinout | Northwest | Northwest |
| Channel Count | 1 | 1 |
| Package | SOT-SC70-5 | SOT-SC70-5 |
| Package (TI Equiv) | DCK5 | DCK5 |
| Vs min (V) | 1.6 | 1.6 |
| Vs max (V) | 5.5 | 6.5 |
| Response Time, typ (µs) | 0.26 | 3 |
| Vos max 25°C (mV) | 4 | 2 |
| Input Range | R-R | R-R |
| Output Type | PP | PP |
| IQ (max) (mA) | 0.01 | 0.0009 |
| IBias (typ) (nA) | 0.005 | 0.002 |
| Temperature Min | -40 | -40 |
| Temperature Max | 125 | 125 |
| Additional Features | POR, Int 4mV hyst, FailSafe, Vout>V+ | POR, Int 7mV hyst, FailSafe, Vout>V+ |
| Auto Qual | ||
| GPN | TLV7011 | TLV7031 |
| Datasheet | TLV7011 | TLV7031 |
| TI Web Page | TLV7011 | TLV7031 |