Other Parts Discussed in Thread: AMC1200, AMC3330, AMC1311, INA146, AMC131M03
Tool/software:
I am working on a project to measure the voltage across multiple series-connected supercapacitor cells using the AMC1300 fully differential isolation amplifier. The first cell in the stack has a voltage of 60V, and I chose the AMC1300 due to its high common-mode voltage (VCM) tolerance, which seems suitable for this high-voltage application.
Application Description
-
Objective: Measure the voltage across each supercapacitor cell in a series stack with Balancing resistor in parallel.
-
Configuration: I plan to connect the AMC1200s in a daisy-chain manner for the differential inputs:
-
The VINN pin of the first AMC1200 (component 1) is connected to the VINP pin of the second AMC1200 (component 2), and so on, to reference each cell's voltage relative to the next.
-
Each AMC1200 is intended to measure the differential voltage across one cell.
-
-
Setup:
-
The first cell is at 60V relative to ground.
-
Each AMC1200 is powered with isolated supplies (VDD1 = 5V, VDD2 = 5V, with proper isolation between high-side and low-side grounds).
-
Issue Encountered
In simulation (using a SPICE model of the AMC1300), the configuration does not work as expected:
-
The simulation shows an unrealistically high power dissipation of approximately 11 kW, which is clearly incorrect.
-
The measured voltages across the cells are not accurate, suggesting an issue with the input configuration or common-mode voltage handling.
Questions
-
Is my proposed configuration (VINN of one AMC1200 connected to VINP of the next) valid for measuring voltages across series-connected supercapacitor cells? If not, what is the recommended approach?
-
Could the high power dissipation in simulation be due to improper handling of the common-mode voltage, given the 60V on the first cell? Does the AMC1300 require additional components (e.g., voltage dividers or clamping circuits) to manage such high VCM?
-
Are there specific design considerations or reference circuits for using multiple AMC1300s in a high-voltage series stack application?
-
Could the simulation issue be related to the SPICE model or simulation setup? Are there known limitations or settings I should check?
Additional Details
-
The supercapacitor cells are expected to have voltages in the range of a few volts each, but the stack starts at 60V for the first cell.
-
I am using the AMC1300 for its isolation and high VCM tolerance, as specified in the datasheet
-
The simulation tool is SPICE model from TI.
Any guidance on the correct configuration, simulation troubleshooting, or reference designs for this application would be greatly appreciated. Thank you in advance for your support! Do no hesitate to recommand me anoither device that could do the job.
Best regards,