Part Number: THS7374
Tool/software:
I'm trying to add a THS7374 to my video PCB design but it keeps failing in circuit.
The power supply is +5 VDC. I have a 1.1uF bypass capacitance across the supply: 100nF right next to the VS+ pin and 1.0uF right next to that.
Pins 5, 6, 7, 8, and 9 and connected to GND. Is it ok to ground the NC pins (7, 8) or must they be left floating?
Channel 4 is driven by a resistor network. The input signal range is 0V to about 910 mV and the network's equivalent output resistance is 778.5R. The output drives a standard video load (150R to GND) in parallel with a divide-by-2 voltage divider. The divider is a pair of 1k resistors to GND.
Channel 3 is driven by the divided version of CH4 output. The input signal range is ~150 mV to to ~600mV with a driver resistance of 500R. It drives nothing for now. The output load is unpopulated.
Initially, I was building the PCB in sections, so Channel 1 and 2 inputs were floating on the first try. But I've tied those off now.
Channel 1 is driven by a resistor network similar to Channel 4. Input range is 0V to about 650mV with a source resistance of about 125R. The output is a standard video load (150R to GND).
Channel 2 is disabled for now. The input is tied to GND and the output load is unpopulated.
Channel 1 seems to be working still but Channel 4 always dies for some reason. (and of course Channel 3 gets a bad input so it misbehaves as well.)
It's like the Channel 4 input goes low impedance after an indeterminate time and drags the input signal down. If I cut the trace between the resistor network and pin 4 of the IC the signal comes back perfectly on the network side.
I've tried DC input coupling, AC coupling (0.1uF) and AC+bias coupling (0.1uF and 3Meg pullup to +5V). And with 3 different devices now. But the IC always fails after some time. It might take a few minutes or half an hour. I'm not sure what the problem can be. I don't think it's a thermal issue...the IC feels cool. I'm out of ideas.