Part Number: LMH5401
Tool/software:
I am using this FDA in a circuit interfacing with an ADC that provides a common mode pin to tie to the LMH5401's CM pin. The ADC's datasheet specifies that its common mode is designed to drive a high impedance load of ≥ 10 KΩ . If a lower impedance load is required, a buffer should be used on the common mode signal.
The datasheet for the LMH5401 provides this:

I just wanted to see if anyone could verify the FDA's CM pin input impedance is high enough that I would not need to include a buffer? Any insight is appreciated - thanks!