Part Number: INA241A
Tool/software:
Dear Support,
I'm using the INA241A2 (gain 20) with a shunt BVR-Z-R0005-1.0 to measure the triangular waveform of a bidirectional current of +-50A.
Mi output after the INA241A2 is a differential output where Vrif=2.5V and the output changes from 1V (-120A) to 4V (120A F.S.)
I was considering to use a shunt with less resistance value, the BVR-Z-R0003-1 but changing the INA241 with more gain INA4241A3 (gain 50)
In this case the differential output is Vrif=2.5V and the output changes from 1V (-100A) to 4V (100A F.S.).
In terms of accuracy and noise what INA should have the best performance? (my circuit have offset and gain calibration)
Thank you
Enrique