Other Parts Discussed in Thread: INA199
Tool/software:
Hello,
I'm designing a current measurement circuit using the INA199B1DCKR for monitoring a DC brushed motor's drive current. Whether driven by DC or PWM, there's a significant difference between the average and peak currents.
Therefore, I'm considering using two shunt resistors: one optimized for accurate average current measurement, and the other for accurate peak current measurement. My idea is to place both shunt resistors in series on the low-side of the motor's drive current path. Each shunt resistor would then be connected to a separate INA199B1DCKR to convert the current into a voltage, which would then be monitored by two AD converters on a single CPU.
Could you please advise if there are any potential issues with using two shunt resistors in series on the low-side with two separate INA199B1DCKR devices? Also, if there's a better approach, I'd appreciate your suggestions.
Thank you.